Is there a way to vary the output voltage of the TPS53355EVM-743?
Ideally I would like to be able to vary the output voltage using a CC3200 and something like http://www.ti.com/product/tpl0401a-10
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a way to vary the output voltage of the TPS53355EVM-743?
Ideally I would like to be able to vary the output voltage using a CC3200 and something like http://www.ti.com/product/tpl0401a-10
Hi John, thanks for the reply.
I have done some experimentation and it so far things are going really well, but I have one question.
Ideally I would like the voltage to go as high as possible, if I am not mistaken, this is 5V for the TPS53355. When I use webench to design a circuit, using 6.5V - 8.4V input, 5V @ 30A output, I get a 0.82 uH inductor, but the TPS53355EVM-743 only has a 0.44 uH inductor. Will this need to be changed out to get the full 30A at 5V.. so far everything is working correctly up to 5V using the current inductor, but I haven't been able to find a load that will use 30A.
Thanks,
Derek