I have used the data sheet reference design and layout guidelines to utilize the TPS62170. the efficiency falls off very sharply below 0.1 amps(20% Low vs datasheet). Any particular things I should look at?
Thanks
Pete
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have used the data sheet reference design and layout guidelines to utilize the TPS62170. the efficiency falls off very sharply below 0.1 amps(20% Low vs datasheet). Any particular things I should look at?
Thanks
Pete
Could you please post your schematic? Could you give the measured values for a point which has low efficiency?
If you click on 'use rich formatting' on the right when you are typing your reply, a full editor opens up with an insert media option.
Thanks Chris
Here is the data
Input voltage VIN= 5V | ||||||||
Test items | load current (mA) | VIN (C56.1) |
VIN Current(mA) (J3.1) |
PP4V4 OUT Voltage (C11.1) |
PP4V4 OUT Current(mA) (R12.2) |
Efficiency (%) | ||
High Voltage Buck PP4V4 | 250 | 249 | 5.00169 | 229.5198 | 4.37695 | 249.1885 | 95.008542 | |
200 | 199.3 | 5.02293 | 182.8042 | 4.37714 | 199.3609 | 95.03577652 | ||
150 | 149.4 | 5.00401 | 137.8649 | 4.37715 | 149.5417 | 94.88157037 | ||
100 | 99.5 | 5.00778 | 92.62563 | 4.37341 | 99.64954 | 93.95482234 | ||
50 | 49.6 | 5.01865 | 48.34521 | 4.37296 | 49.77986 | 89.71990717 | ||
40 | 39.6 | 5.00082 | 39.55464 | 4.37336 | 39.7952 | 87.98472098 | ||
30 | 29.6 | 5.00525 | 30.12694 | 4.37548 | 29.83321 | 86.56550988 | ||
20 | 19.7 | 5.00333 | 20.58255 | 4.37675 | 19.91097 | 84.62249603 | ||
10 | 9.7 | 5.0093 | 10.89389 | 4.3798 | 9.922079 | 79.63370691 | ||
8 | 7.5 | 5.00649 | 8.902365 | 4.38161 | 7.919515 | 77.85626317 | ||
6 | 5.8 | 5.00464 | 6.994271 | 4.38254 | 5.951071 | 74.50848316 | ||
4 | 3.6 | 5.00745 | 4.937832 | 4.38549 | 3.946546 | 69.9974732 | ||
2 | 1.8 | 5.00699 | 2.950119 | 4.38626 | 1.944892 | 57.75287419 | ||
1 | 0.7 | 5.00356 | 1.94571 | 4.38691 | 0.9569108 | 43.11942471 |
Hi Chris
We have two supplies: Normally from a 12v source, the second is from a USB supply hence the TPS62170.
I tried to send the schematic in PDF format. The paste from word button didn't work? Should I use aanother method?
Pete Peterson said:I tried to send the schematic in PDF format. The paste from word button didn't work? Should I use aanother method?
Pete,
There are two different options currently available for attaching files. See this article here for a how-to and walk through of each option.
Hi Chris
Well you certainly have addressed the issues for me for which I am grateful. My circuit is not battery powered and I have been leery of the 2.2uH inductor. You are right , the efficiency at higher currents is certainly more important for temp. rise issues etc.
I will try the 3.3uH inductor and see if it props up the efficiency a bit.
Thanks for all your help - TI is lucky to have you!