Hi there,
I 'm member of a university team and we are trying to build a charging system for supercapacitors. So we use three PTN78020HAH in parallel connection each of them has an adjusted output on 15V. Two months ago one of the buck converters was burned during our test. After debugging the whole system we discovered that the burned PTN78020HAH has a little higher output voltage(0.2V-0.4V) than the others so it was working more than them.
After that, we replaced the adjustment resistors needed with new that have tolerance 0.1% as mentioned in the manual. Then, two buck-converters have output voltage 14,98V and the third 15,01. We guessed that it was a very little difference and started the tests again. Unfortunatelly after some tests, that buck converter got burned again.
Is that little voltage difference responsible for this or it is our mistake? And if yes, could we use just one resistor for the three buck converters(they have common ground) to have the exact same output?
Thank you in advance,
John