I'm currently trying to bring-up a new design, but am having some difficulty with the TPS65400. We've design this particular supply to that two of the rails will turn on automatically, while the other two are enabled by an FPGA later on. The intent of the design is to work as intended without the need to program the controller, ie it should work stand alone. Here are some waveforms to help illustrate what we're seeing:
This screen capture shows the 5V input (purple), 3.3V output (yellow), and the 3.3V SW node between the TPS65400 and the inductor (pink). There are a few things to note here:
1) 5V turns on cleanly
2) The 3.3V rail overshoots the 3.3V set point and reaches 5V on when powering up
3) The 3.3V rail settles at 3.3V after some time
4) The 3.3V rail SW node never appears to switch, but looks as if it is regulating linearly
I tried putting some extra loading on 3.3V and noted that the output voltage decreased to 3.1V, so it appears that the 3.3V phase is not actually regulating.
This image shows the other phase that should turn on automatically. It is a 1.5V rail. In this image the rails are represented as follows: 5V (purple), 1.5V output (yellow), and 1.5V SW node (pink). Note that:
1) 5V turns on cleanly
2) The 1.5V output actually regulates to 3.5V
3) The 1.5V SW node switches as expected and the Pulse Width increases as expected for soft start
I measured the feedbank pin for this rail with a volt meter and found it to be 1.866V, so it appears to me as if Vref is set to 1.87V, but again, we haven't done any programming of the part, so I expect Vref to be 0.8V.
Please let us know how this behavior may be explained, and what else we can try or look at to solve the problem. I'm attaching the relevant schematic page from our design.
Please note that we would like to solve this problem quickly.
Thank you for your help.
Best Regards,
Kevin