I have implemented the TPS61025 to boost to 3.3V from a two-cell alkaline battery input. With fresh batteries (VBAT = 3.0V), the output voltage is approximately 3.25V, but when the input voltage starts to drop the output also drops. The system current draw on this regulator is less than 200mA. I have followed the datasheet and I don't see any reason why the circuit is not working. Any help would be appreciated.