I am looking for a high efficiency solution that will output 48V @ 4A max with input of 11-30v. Any tricks to coax that much wattage out of the latest chips?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you explain why specifically?
WEBENCH® LM5122
Does not work with those parameters.
Let's assume that average current draw is fine with TPS43060.
However, at time 0, a reserver capacitor will present a short circuit at full voltage. That could be 1,000A equivalent current. Can soft-start time be extended to 5 seconds so that current draw can be reduced as the cap charges? Also, do you recommend using inductor DCR current limiting or resistor current limiting for this case? I'm using a 26A inductor - why not use that approach?