Hi
My customer has question at TPS54325_Pre-Biased operation.
Vin=5V
Vout=1.8V
Pre-Biased≒1V
At this time,SW stops at Startup.Please see the attached file.
This operation is starting specification at the time of Pre-Biased?
Regard.
T Kishi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My customer has question at TPS54325_Pre-Biased operation.
Vin=5V
Vout=1.8V
Pre-Biased≒1V
At this time,SW stops at Startup.Please see the attached file.
This operation is starting specification at the time of Pre-Biased?
Regard.
T Kishi
It is hard to tell from that waveform. Is the slow start time completed already? Can you show both a zoomed out and zoomed in version? What is the load current?
Hi John
Thank you for replay.
Load current =0mA.
The SW stop happen just before and just after the slow start is complete.
And,SW stop does not happen when the output is completely stable.
Attached the zoom version of waveform.
Regurds
Actually I was looking for you to zoom in the other direction as well. I need to see that area of interest closer in. I may be able to answer anyway, but it would help.
Thanks.
Hi
Measured waveform of when there is no Pre-Biased.
Please see the attached file.
Is this will normal Operation?