Hello,
I was planning to use the TPS53515 in a new design, and recently became aware that it has latching undervoltage protection. For the application I am using it in, I need this converter to have a hiccup or auto-retry on its protections. I was not able to find a pin compatible replacement without latching protection, so since the layout is already far along, I would prefer to add a supervisor or sequencer or monitor, or hot swap controller, or something else that I can use to automatically reset the converter.
A bit more about the application: Vin = 12V, Vout = 5V and 3.3V (using two TPS53515), Iout <5A (each converter). The 12V supply is fed in from another card.