I made the attached diagram that uses the switching regulator TPS40055. The features of the converter are the following: Vin = 18V to 32V; Vout = 13V; Iout MAX = 20A. Without load connected, the output voltage at the pin "+12V1" is 13V but with 10A load current, (half of the maximum load), the Vout drops to 10.5V.
My question is the following: It is normal that the voltage drops so much?
Many thanks