Hi,
We have been using the TPS63002 for fixed output voltage of 5V and have used the resistor and capacitor values as mentioned in the typical application circuit of the datasheet.
We've have faced these issues often (Unfortunately I couldn’t manage to measure the currents)
Getting an output of around 2 or 3 V instead of 5V OR No output at all at the Vout pin
After placing new ICs, these seemed to work but would fail again with same problems after a few days.
Going by the frequent failures we narrowed down the reason as a thermal one. We think not enough contact between the thermal pad of PCB and the IC was taking place due to hand soldering.
- 1. What kind of thermal pad would you recommend when soldering these ICs by hand? Would you recommend a through hole thermal pad instead of the SMD one for this IC?
- The connections especially - EN to VIN and PS/SYNC to VIN , VIN to VINA use different resistor values in the EVM and typical application circuits. Could this be a reason for the issues? Which circuit would you recommend we follow?
- We are using Li-ion battery with a max voltage of 4.2 V as an input. Would you suspect not grounding the PS/SYNC but making it high (as per typical applcn circuit) causes issues for battery powered application circuits?
Thanks !
Sowmya