Hi,
I want to charge up a capacitor using a boost with a LM5121. To keep the charging current constant I use a INA169 current sense monitoring sensing the boost´s input current. The INA169 output is connected to the Error Amplifier. So the input current is regulated, not the output voltage. To turn off switching (with a comparator) when the output voltage is reached and to turn on again when it falls I see 3 possibilites:
1) using the UVLO Pin: if this pin is pulled to ground, the LM5121 stops swtiching, but shut-down-wake-up takes to much time (about 400us I measured on the evalboard). Pulling UVLO to 0,5V...1,17V also stops switching immediately, stand-by-wake-up time is good enough for my application (about 20us I measured on the evalboard). But pulling UVLO to the required voltage with a diode as recommended in the datasheet is a very precariously way - over the temperature range -40...+70°C. I have designed a solution with a an external voltage reference, but it is not a "keep it simple design"...
2) using the SS-Pin: pull down the SS-Pin works fine and fast, but I want to have the soft-start only during start up and not during normal operation (output capacitor discharged by pulsing load and reloaded again). I thought I can avoid th Css, because the current is regulated. But Css is also needed to ensure the BST voltage for the High Side FET. So maybe also not a recommended solution.
3) using the FB-Pin: I pulled the FB-Pin to 2.5V to switch off and it works fast switching off, but disconnecting the 2.5V and the regulator starts with a delay of 2ms and needs a lot of time (ms) to regulate (in my simulation).
What Pin would you recommend to use for fast turn-on/off switching?
I appreciate any comments,
br
Andy