Hi
I would like to know average quiescent current at ultra-low load current.
I'm considering 12V/2A output system, and input voltage is 24V.
However, almost, IC that becomes the load is in a sleep state, it will sometimes cause.
At waking time, the load current is 100mA, when sleep is 1mA.
During the waking time, the pulse of the load current 2A occurs.
Pulse width is about 500us from 100us.
I would like to know average quiescent current.
Since the ratio of the time that is happening and the sleep time required to consider,
the average current is averaging the quiscent currents in each load current by duty ratio.
In the case 1mA or 100mA, I think that it will be operating in pulse skip mode, how much current consumption.
I used Webench, consider as shown in the following figure 12V, the circuit configuration of a 2A output.
Is there a way to know 1mA, the average current consumption during 100mA in this circuit?
If the efficiency of the results of at 100mA, but I think that it is calculated back to be able to calculate the average current,
in Webench, it does not come out only up to 200mA efficiency of simulation results.
Please let me know if there is a way to know the average current.
In this case, sometimes 2A of pulse current is generated.
How it would be considered fever?
I believe if the pulse width is short, the heat is not completely raised, and therfore I want to know the formula,
such as showing a relationship between heat and pulse width.
Thanks.