I'd like to use the LM46002 as an LED driver. The standard 1.01V is much higher than I'd want to have across a current sense resistor - my hope is that I can apply a fixed 100mV to the SS/TRK pin, and the part will then regulate FB to 100mV, but otherwise operate normally. Is that the case?
And if THAT works, I'd like to then control the voltage on the SS/TRK pin to implement a brightness control. Will the part follow the SS/TRK pin both up and down?
Any concerns about this? Or is this badly misusing the SS/TRK pin and will make the part mad?