This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2572

sir,

i want to know input and output voltage, current of EVM module. Is it possible to vary the output voltage.

www.ti.com/.../slvu180.pdf

  • The input voltage is -48 V. the output voltages and currents of the various modules for the POL converters are given in the schematic and table 1. They are somewhat adjustable, but that circuit is specifically designed to support Advanced Telecommunications Computing Architecture (ATCA). U12 and U8 do not have any connections to the adjust pin.