Hi everyone,
I am trying to find out what is my maximum output current when using TPS61175PWP to both 5V to 12V and 5V to 24V.
If I check the formulas showed in page 12 (5) or page 13 (8), with data provided in the example just below formula (8), and i perform the calculations, the result is not the expected, which the example describes to be 1.2 A.
My application data are:
- Vin: 5V
- Vo = 12V & 24V
- L = 15 uH.
- f = 1.2 MHz.
- Schottky forward voltage: 0.6 V
¿Which formula should I use to perform the calculations about maximun output current?
Thank you in advance,
Carlos Gonzalez