IIn our project we required different type of Supply voltage 5v,9.9v,12v,15v,18v,24v,-12v with 2Aload,.Could you guide me which one of the TI IC suitable for our requirement. Now we are going with TPS5450&tps5430,POWER SUPPLY 1.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
IIn our project we required different type of Supply voltage 5v,9.9v,12v,15v,18v,24v,-12v with 2Aload,.Could you guide me which one of the TI IC suitable for our requirement. Now we are going with TPS5450&tps5430,POWER SUPPLY 1.pdf
voltage like 12V,15V,18V,24V & tps5450/5430 is suitable for 5V&3.3V supply. Negative voltage -12V is generate by using Tps54540 its ok or not? . Today i have install the switch pro simulation software . i have simulate 12v,15V,18V,24V voltage, when we get the simulated output PWRPD pin pulled up 5V using
10k resistor its necessary or not?
PWRPD...are you referring to the powerpad? It will be connected to GND. It is the thermal heatsinK for the IC.
Thanks for your quick reply,
Here along with attached switch pro simulated output for 12V. Please find it.
Dear sir,
Sorry for the late response . As we discussed earlier i have designed the schematic as well as board layout. Here i attached schematic & board files for your reference schematic and board.zipschematic and board.zip,send your feedback.
I have query,
1. Now, i have used different voltage power sources and in layout common GND filling method .whether i need to use to give isolated GND for each voltage source, could you able to give suggestion?
2. could you send
a) shape to shape clearance of board layout
b) signal to signal clearance of board layout
3.As per TI datasheet design layout guidelines,
"Power Supply Recommendations
The design of the device is for operation from an input voltage supply range between 3.5 V and 42 V. Good
regulation of this input supply is essential. If the input supply is more distant than a few inches from the
TPS54240 converter, the circuit may require additional bulk capacitance in addition to the ceramic bypass
capacitors. An electrolytic capacitor with a value of 100 μF is a typical choice"
just i want to know whether i need to add additional capacitor depends on distant from input supply or not?
give me your suggestions
NOTE...I cannot respond to this post for some reason. It will be few days before I can respond if it is not fixed soon. Just FYI
Dear sir,
Sorry for the late response . As we discussed earlier i have designed the schematic as well as board layout. Here i attached schematic & board files for your reference schematic and board.zipschematic and board.zip,send your feedback.
ti.zipI have query,
1. Now, i have used different voltage power sources and in layout common GND filling method .whether i need to use to give isolated GND for each voltage source, could you able to give suggestion?
2. could you send
a) shape to shape clearance of board layout
b) signal to signal clearance of board layout
3.As per TI datasheet design layout guidelines,
"Power Supply Recommendations
The design of the device is for operation from an input voltage supply range between 3.5 V and 42 V. Good
regulation of this input supply is essential. If the input supply is more distant than a few inches from the
TPS54240 converter, the circuit may require additional bulk capacitance in addition to the ceramic bypass
capacitors. An electrolytic capacitor with a value of 100 μF is a typical choice"
just i want to know whether i need to add additional capacitor depends on distant from input supply or not?
give me your suggestions
I still cannot respond to your thredd...I suggest you start a new one.
I could not open your schematics at all and while the brd file did open, redraws were painfully slow at several minutes, so I could not examine it closely.
- I almost always use a common ground plane on an internal layer for designs like that (maybe 2) You will definitely want some exposed copper ground under each IC connected by thermal vias to the exposed thermal pad. Be generous with this and it will pay you back later. You may want to use small isolated grounds for sensitive analog returns like the GND termination for the feedback an COMP. It can be electrically common to the main GND plane, just connect to it at a single point for each small analog GND island or etch run grouping. This keeps switch currents away from them.
- I am enclosing the design rule settings I personally use. With in reason, they are determined by you own particular PCB vendor and any additional constraints your company may have. I can't guarantee they will meet your needs, but it is what I use.
- Based on what I could see of your layout, I think it would be best to add some bulk capacitance. Maybe one each at the head of each input voltage etch rail. Another thing, Those fill areas for VIN seem rather narrow. I would probably widen them. Also you are using just wide etch for the switching node of each regulator. Not generally a good idea. I would use small copper fills.design rules.pdf
Hope this helps.