From our customer:
We have a SEPIC design based on a TPS40210, and I’m trying to reduce emissions from it. Overall, it is not bad but we are getting some AM band (roughly 500 kHz to 2 MHz) emissions that we are trying to reduce. We can get them under our limit line if we place a shield over the transformer, so the emissions are coming from the transformer itself. A shield is not a great production solution, so I’m looking for alternatives. The transformer is a bobbin/drum style, and I think it would help if we could use a toroidal transformer instead. I’m going to probably order a couple toroidal transformers to try.
We originally started with a Coilcraft part number MSD1278T-183MLD, and now we are using Vishay part number IHCL-4040DZ-5A 33uH, but both have similar levels of emissions. These both are shielded coupled inductors, but the shielding is done with ferrite, and I think it just isn’t very effective at low frequencies. If the shielding is ineffective, then it basically becomes a loop antenna I think.
I was just wondering if TI has recommendations on transformers or coupled-inductors for this SEPIC architecture. I’ll continue with our own experiments, but let me know if you or any of the power supply experts at TI have any advice for this.