could someone here help me find a dc dc converter, seems i could not find the one i want here
input: 3.6V (fixed)
output: 3.6 ~ 7V which can be controlled by microcontroller, either I2C or SPI
Max Iout around 1.5A
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
could someone here help me find a dc dc converter, seems i could not find the one i want here
input: 3.6V (fixed)
output: 3.6 ~ 7V which can be controlled by microcontroller, either I2C or SPI
Max Iout around 1.5A
thanks
hi Jasper, thank you for your message
the vout is from 3.6v to 7.1v. because the product will allow the costumer to modify the voltage themselves by push a button, and we prefer the voltage could be changed from 3.6v to 7.1v by 0.5v increment or so
Hi Jasper,
we are currently using our device to burn an electrical cigarette's atomizer (2.4ohm~ 2.6ohm), and the current can be as much as 1.5A.
we need a boost converter to provide a 3.6V to 7V voltage from a 3.6V battery and allow the user to modify the power by just pressing a button in around 0.5V increment.
Today an engineer told me i can choose a PWM converter to make it true. so dear Jasper, our project is like this, do you have any solution or links could help us on this
Thank you
thanks Jasper,
it was my mistake, seems the atomizer resistance will rise up a little bit as the voltage rising up. usually 2.5ohm ~ 3ohm. and the output current could be more than 1.5A, probably around 2.5A
a PWM signal + RC filter seems to be a good solution, would you mind provide some diagram/schematic of it? or could you provide any TI's chip which has such functions?
Thank you again
Robert
following could be a solution. you can apply an EVM to verified. i can do some tests to make sure the TPS61088 can support 3.6V in and 3.6V output application if the solution is OK for your.
why the input voltage is fixed 3.6V? as i know, the input power of this kind of product should be a battery.
may i know the part number of the atomizer you are going to used. or there is a datasheet of the atomizer you could share. thanks
Jasper Li