I am using the TPS61040 switching regular to boost an input voltage of +5VDC to +24VDC. I would like to consume 160mA at the output and this regulator is listed as having an internal switch current of 400mA however neither the calculation or application give the desired 160mA.
What inductor size should I be using and what switching frequency will this achieve? Is this even possible with this regulator?