Hello,
I'm developing a device which uses the TPS62120 to generate a -1.6V supply rail for operational amplifiers. The performance in terms of efficiency, noise, regulation and so on is entirely satisfactory, but the circuit will not start up under certain conditions.
We have tested the converter with either the EN connected to VIN or the EN connected through a level shifting circuit as described in SLVS478B, pargraph 2.1 and under certain loads the converter will not start up.
I have tracked the issue down to the fact, that there is slight leakage from the 3.3V rail to the -1.6V rail, which produces about 12mV of positive voltage across the converter output capacitor, which clearly holds the converter from starting up. As soon as the output capacitor is shorted (for example with a tweezer) the converter starts up and works reliably. My colleague also found, that introducing noise into the circuit via a loop of wire carrying a ~20kHz sine wave will also prevent it from starting.
So far we have been unable to find a solution that would work in all conditions and be robust against EMI, which may force us to seek other alternatives and we'd like to avoid this because we already have the TPS62120s in the circuit generating other power supply rails, and it would be convenient to reduce component variety on the PCB.
Please see below the circuit we are using.