Total power at load is 5V @ 3.244W. Allowing for 20% inefficiency all in the controller ignoring inductor and traces, input power would be 4.055W. Power loss in controller is 1.014W. With Rtheta-JA = 87.9C/W without heatsinking, Tj = Ta+89.13C. At Ta = 70C, Tj = 159.13C. Considering the metal on the board and attempts to heatsink the controller, that Tj should be acceptable.
I've had 2 controllers blow. One could have been an accidental cable short. The controller is well filtered and input and output caps are placed very close to the IC. No ringing. Vin = +15VDC and it appears clean. Still have to check for power-up spiking on Vin since the IC has a 17V limit. Spec notes says the device isn't guaranteed to operate properly above the recommended +17VDC(max) input even though abs max is +19VDC. The device has both over-current and over-temperature protection.
Am I missing something? What changes do you recommend?
Thanks,
Mike
Layout, 2-sided PCB, 2oz copper. Bottom layer is seen looking thru the Top layer.