Hello,
I built a product using the TPS62175 step down regulator. The prototype is not working and I don't understand why. Can you help me find the problem?
Cin: 10uF/50V MLCC
Cout 47uF/16V MLCC
Lout: 10uH
Vout: set to 3.3V with 47K/150K resistors
Vin: 24V
Enable: connected to Vin
Sleep: connected to Vout
The output voltage is 0V. The switch gives pulses of 300ns at a frequency of 1000hz. There is no short circuit on the output.
FB = 0V
The chip seems to be in sleep mode. But for that it would have to assume that Vout is ok. But Vfb = 0V.
What am I missing?
Thanks in advance.
Ronald