Hi,
I tried TPS61040 and TPS61042 eval boards for 9V output and 200mA output current using rheostat. Not able to get the line voltage regulation. i varied the input voltage from 2.2V to 5V. Observed output voltage has 1.5V worst case difference.
TPS61040 - FB pin (R1 = 220k; R2=36K)
TPS61042 - RS pin connected to 1.2 Ohm; RS and FB are shorted.
Thanks,
Siva