Hi,
didn't know where to present the following question, so i'll try here :)
I'm having an ear tag PCB (i.e. very small 30x30 cm). I want to give regulated power to 2 main blocks-
1. micro SD card which need 2.7v- i thought of using the boost converter TP61030
2. Rest of the circuit- MCU, CC1121, MEMS, Gyro- I need 2v (to stabilyze the sensors) , using TP6247 (this was tested already, with the down converter and the circuit is working fine)
I'm using a 3.1v battery for the circuit. this is a logger R&D circuit, not for production!
My Q is- can I use both on the same PCB?
Thanks in advance!
Ram