I am trying to apply the LM25011 to a project and can
simplify testing by clocking it either below 150 kHz or
between 300 and 500 kHz. The data sheet gives examples that
run it at 1 MHz and specifies minimum on- and off-times,
thereby implying a maximum frequency, but I can find nothing
there or on any forum for running at a lower frequency.
Is there a fundamental lower limit on switching frequency
(other than the value of RT, which comes out to 1.2M with
5 V output)?