I tried to re-configure the PMP7390 design to fit a long/narrow PCB, but cannot get it to work. I've attached the schematic and board images I used below, I hope someone can point me to my mistake. I get 3.3V from the VDD pin of the TPS40170, but the input to the TPS2511 is only reading 0.58V.
Red traces on top, blue traces on bottom, all components are on the top.