Hi, team
My customer's design are below
・ Vin= 8V-16V±10%
・Vo=5V±2% and 3.3V±2%
・Ripple =Vout*5%
・Io:7A(typ.)/10A(MAX)
TPS51220A' mode is current mode and external register sensing and no-droop .
Then, please how to set the phase compensation.
I do not understand how to set the phase compensation (datasheet P31 eq17).
So customer's Rgv is 0ohm in the cirucuit, then Cc=Co from eq17.
Best regards,
Kenji Ito