Hi,
I have a TL497A set up to convert +5V to -19.5V. The problem I am running into is that the output voltage drops to -14V or so when the load is greater than a few mA. I need to be able to supply ~20mA. Any thoughts would be appreciated.
Thanks,
Andy
Values:
Current limiting resistor: 2 ohms
Resistor 1: 18.3 k-ohms
Resistor 2: 1.2 k-ohms
Inductor: 470uH
Timing capacitor: 270pF