I am using the LM5576 to convert 27....40V to +24V as in the webench circuit below.
As 1.2A is a peak output current only with an average output current of 250mA I made the circuit more lightweight using the Quick start guide to recalculate values. See schematic below
L1 became 94uH (2x 47uH in series)
Rt 43k
CRamp 1nF
Rramp 100kOhm
Css 22nF
Rfb2 27k8
Rfb1 1k5
Cout 225uF
Ccomp 6.8nF Rcomp 30k0 Ccomp2 not populated
This configuration works OK at higher loads, but fails during light load conditions.
Simulating the circuit with tina shows that there is an overshoot at startup, which leads to some ms of inactivity, which potentially leads to undervoltage lockout caused by losing the bootstrap voltage.
Reducing the Output Cap to 20uF together with using an modified compensation network solves this problem in simulation, but is far away from calculated values:
Cout 20uF
Ccomp 22nF Rcomp 82k0 Ccomp2 22pF
Simulating the circuit gives good results between 6mA and 1.2A load.
Can I safely use these values, or are they outside the defined LM5576 range?
B.R. Ralph.