I'm doing test circuit Boost voltage. I see on the datasheet of some kind that me see IC Boots voltage (LM2586) through the circuit structure as shown in the attached Figure. I see it with foot ON / OFF but if you see the way infected OFF circuit as shown in Figure the IC but inactive, the output is not Boots up but output voltage also exists that voltage which runs from input voltage across the coil. That is equal to the input output when IC OFF. So the question I want to pose is not for IC Boots to the operation as will the 0v output instead it up with the input. The forum you have any idea or solution to help you with!
Thank you very much.