Hi all.
I would like to know the min and max value of soft-start time.
The FPGA that my customer is using is defined 0.2ms~50ms(0~90% rise),
but TPS51219 is 1.1ms(0.4ms : delay 0.7ms : soft -start time(0~100%))
Please tell me min and max soft-start time.
I would like to give your answer as soon as possible.
Best regards,
Sho Ogane