Hi all,
I have three questions about TPS53915.
(1)My understanding of the power up sequence of TPS53915 is as follows.
If the power supply(VIN) of TPS53915 is turned on without sending any PMBus commands,
the entire contents of NVMs will be stored to the operating memories,
and TPS53915 will work with the stored memories(the operating memories).
Is my understanding correct?
Or, is the RESTORE_DEFAULT_ALL command needed?
(2)I understand that the values written on NVMs at the time of shipment are the values described
on the data sheet(described as TI default).
for example)
Is my understanding correct?
(3)If the PMBus commands are not used,can SDA pin and SCL pin be left floating?
Best regards.
Tsuyoshi Tokumoto