I've built this circuit: http://i.imgur.com/7dE8amh.png where some BPW34s tiny solar cells charge a capacitor up to 2V. But it doesn't work, the input stops at 0.8V, maybe because of the very slow startup voltage ramp, because the BPW34s provides only a few 100 uA max.
Does TI have a boost converter IC which works for this application and which is maybe even cheaper as the Maxim part? The requirements are very moderate: max 10 mA output, output voltage can vary between 3V and 3.6V, needs not to be efficient, but cheap. I found the TPS61221, which exceeds my requirements, but does it run with this slow supply voltage ramp? In my final product I plan to use even bigger capacitors, so that it will ramp up in an hour or so.