This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2734

Other Parts Discussed in Thread: LM2734

I have a customer that is failing Class B FCC , Radiated EMI by 5 dB, and it appears to be coming from the LM2734. Vin = 12V, Vout =2.5V, Iout 800mA.  Boost voltage is 5V from another source. The layout is good, Inductor is 4.7 uH, and claims to be shielded.   Running at 1.5 MHz.  Waveforms look right. Similar LM2734 circuits on same board with less load don't radiate as much.  What do you suggest ? Thank You !!