Looking for boost converter for LED drive for 8 leds (2PX 4S).
Vin(mini)=1.8V
Vin(max)-5V
Vout=17V
Switch Current>500MA
Low cost
I found theLM2623.
Any other recommendation
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello, look at the TPS61040 family. This has 1.8V input operation. You can configure it for a single string of 8 LEDs, or you can parallel two strings of 4 LEDs and tie the cathodes together at the current setting resistor.
Thanks
Travis
Hi,
LM2623 is a simple boost without LED driver in it, so there won't be brightness control and adaptive boost voltage control to reduce power loss. Its package is even bigger than TPS60142. I think this family is only option can support this low input voltage range.
The closest device we have for this application is the TPS61500.
Thanks
Travis