Dear support member,
My customer used TLV62150.
Output voltage range of TLV62150 has become 0.9V ~ 5V.
When output voltage 5V,
Can you use the DEF pin high?
5.25V (5V + 5%) is more than output voltage range.
Best regard.
Bob Lee.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Michael Helmlinger,
Thank you very much for reply.
May I ask add a question?
Datasheet 1 page and 5 page.
It has been described as 5V,
why is it has been described as 5V?
Do not been described as 5.25V?
Could you teach reason?
Question have attached file.
Best regard.
Bob Lee.
Dear Michael Helmlinger,
Thank you very much for reply.
Your answer "It is ok to use the def pin to get 5.25V on the output."
Why datasheet is not has been described as 5.25V?
Could you teach reason?
Best regard.
BoB Lee.