I am having problem with your TPS63031. For the start: schematic is exactly the same as in datasheet, PCB layout is also the same. Load current is 30mA.
Problem is: when input voltage is bigger then 2.9V everything is ok i see 3.3V on output. But when supply voltage is lower then 2.9 V output is unregulated(it is lower than supply voltage and rises with supply voltage).
I tried to change suply voltage from 1.8V to 4.5V. From 1.8V to 2.9V output is unregulated and supply current rises up to 0.4A. When i reach 2.9V supply current falls and converter starts to work normally.
What can be the reason of such behavior?