Hello.
My customer is currently in considering TPS62235,now.
My customer have been requesting a device with over 80% Efficiency under the following conditions.
So, please tell me about Efficiency of the TPS62235.
※This data without the data sheet
※WebBENCH also non-compliant
Please help me!
<Conditions>
・VIN:3.6V
・VOUT:1.2V(Fixed)
・IOUT:0.05~0.2A
・Target EFFI:over 80%
・MODE=VIN(Only PWM)
・L = 2.2 uH MIPSZ2012 2R2 (2012 size),
・COUT = 4.7 uF
Could you help us?
Best Regards,
Pokkun