There is an error in my PCB layout concerning TPS63060 that leaves Pin 7(GND) open. The PGND pad is connected to system ground. I measure a low resistance from Pin 7(GND) to PGND which I assume the two are connected internally. The circuit functions as expected. Are the grounds internally connected and do you think it is OK not grounding Pin 7 externally?