Dear all,
1) My requirement is DC-DC buck converter with Vin 55V to 85V & output is Vout = 33V , iout = 22A.
2) Can i design this with LM5116WG.
regards
M.Sreenivasan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
1) My requirement is DC-DC buck converter with Vin 55V to 85V & output is Vout = 33V , iout = 22A.
2) Can i design this with LM5116WG.
regards
M.Sreenivasan
HI Sreenivasan,
These design parameters can be done. There will need to be a lot of care when selecting components and doing layout. Since the design calls for 726W it would be a choice to use multiple phases. Here is a good reference design that will help implement your design. Also check out the quickstart calculator as it will help speed up some of the basic calculations.
Thanks,
Garrett