Hello Everyone,
I used the webench to create a 12v to 3.3v output @3.5A using the TPS54625,
When i power the supply up without any load, it outputs 3.34v, which is fine, but as soon as i put a load on it, it instantly drops to 1.9-2.0v, the load is about 2.4Amp at start up,
I Copied the schematic 1:1 from the Webench, and the board layout is pretty much the same. I have done the same for 2 other voltages, 5v and 12v using 2 different products without any issue.
The only thing i could see wrong after first powering it up was the no load voltage was about 2v with the resistors that webench and the datasheet suggested, so that might be a sign of a faulty IC?
Im really not sure whats wrong, This is my first project like this so i wouldn't be surprised if its my mistake somewhere, ive spent the last 5-6hours re-reading and re-checking everything and it all looks good. The PCB has no faults, the values of caps and resistors are all correct and the 12vin is stable.
Any help would be greatly appreciated.