I'm trying to program two TPS65400 with USB2ANY adapter interface. The TPS65400 devices reside on a customized board, sharing the same PMBus. When I launch PI-Commander (0.8.5), there is a popup message saying " Incompatible FTDI device drivers have been detected. To resolve this issue, please exit the program and install compatible drivers which are bundled with this application. The driver installer is accessible from the "PI-Commander-0.8.5" system menu. Acknowledge"
I did that and re-launch the program again, then the SW says no device detected. Can anyone tell me what the problem is? Thanks. --Nikko