Would appreciate some advise for preventing damage to the TPS40170 for a battery charging application.
Vin is only supplied during charging. While not charging, the TPS40170 is not enabled. When a battery is connected to the regulator output, the track going to the SW input blows and the TPS40170 is destroyed. The absolute maximum for the SW input is equal to Vin. In this scenario, Vin will be a diode drop below SW (via HS body diode).
I can prevent the damage by having a diode on the regulator output. However the power dissipation from this is an issue for the design. A synchronous buck design was used to minimise heat to start with.
Testing has been problematic/limited, as the damage to the PCB track makes it very difficult to replace the device.
Any alternatives would be appreciated.