Hi there,
I have an acoustic application that draws low currents but is susceptible to the pulse burst repetition frequency (about 50kHz) of the converter. That is why I would like to use the forced PWM mode (PSP = PSN = low). Is there an aid to calculate new coil and perhaps control loop compensation components for a given Iout (at Vout +15V and -15V)? Or am I on the wrong track?
Webench designer does not seem to offer this mode for calculations.
Acutally the current at the primary Vin = 5 V rises about 50mA for the forced PWM mode. Changing the coils to 12µH alone did not help to get rid of the bursting in power saving mode nor did not change much in respect to the rising primary current.
Thank you for your help!
Best regards,
Olaf