Hi sir,
I have a question about the TPS65286 operation temperature, I have test TPS65286 as below condition, I want to check this temperature calculation is correct or not.(99℃ is real measurement on our MB TPS65286 by thermal imager)
Vin = 20V
Vout = 5V / 4A
Eff.= 80.03
Pd = 4.88W
Tj = TA + ɵja*Pd = 99℃ + 35.6*4.88 = 272℃, but it seems over absolute Tj, is this calculation is right?
Thanks!
Jeff