Hi Team,
I understand that the maximum voltage of SS pin is 0.779V(it is maximum voltage of VFB).
Is my understanding correct?
And, I have one more question.
I simulated the following conditions using "TINA-TI".
As a result, the voltage of SS pin reached around 6.0V.
I guess that "TINA-TI" has a bug.
Is my understanding correct?
[Simulation conditions]
Vin=8.4V
Vout=5V
Iout=3A
Regards,
Kanemaru