Hi Team,
Is it possible to operate in a parallel configuration of some TPS53647s with current sharing?
If the answer is yes, my customer considers to use TPS53647 for the following specification.
---------------------------------
Input voltage: 10~14V
output voltage: 1V
output current: 200A
---------------------------------
Best Regards,
Yaita / Japan disty