Hey,
I'm experiencing quite strange behaviour while using the TPS564201.
I have designed a circuit very similar to the datasheet suggestions. Vin is 12V from a stabilized source. Vout is configured to 5V (I have a second configuration with 3.3V showing the same behaviour).
Cin is 22 µF with 35V max, Vout is 47 µF with 20 V max. C_boost is 100nF. The feedback resistors are 56kOhm and 10kOhm (should result in about 5 V). The inducance is 3.3µH as recommended.
I double checked the layout to be according to the design example in the datasheet.
When I applied a voltage (as mentioned 12V stabilized) to the input rail, I got a short circuit on the output side. I then varied output impedance, to rule out any open load stuff, which didn't change anything. I did a oscilloscope measurement on the output side and it turned out that the dc/dc controlls the output voltage to 5 V for a period of about 10ms and then goes to short circuit. I am wondering ehy it behaves like this, since it seems that everything is correct for a few milliseconds and when the output is stable, it goes to undefined behaviour. I checked the output and input for shorts and/or strange impedances but everything looked okay.
I hope you guys can give me some tips.
Thanks in advance!