We intend to use TPS51631A to convert from 5V to 1.8V.
In the datasheet it is said that conversion voltage range goes from 4.5 to 28V. Regarding VBAT, recommended operating conditions are -0.1V to 28V.
However, there is the following sentence in page 33 of the datasheet: "VBAT does not have a UVLO function, so the circuit operates with power inputs as low as approximately 3xVout".
From that sentence, we understand that VBAT should be at least 3 x 1.8V = 5.4V. What is the relationship between VOUT and VBAT? Would the circuit work with VBAT = 5V? Can you confirm if operation with VBAT = 5V is possible for VOUT = 1.86V maximum?
Do you have any reference design with conversion voltage / VBAT = 5V? All reference designs that we have seen apparently convert only from 9V-20V.
Thanks in advance