Hi to all,
Is there any possibility to damage internal regulator of LM51116 ?
I fed VCCX with output voltage of 13V, and VCC with input voltage of 20..40Vdc.
I utilize LM5116 to charge a lead acid battery : when battery is very low voltage, the LM5116 works in current limit condition. If the input voltage ripple is high (about 5Vpp) the IC LM5116 will damage..
With LM5116 broken, I found Vin on VCC pin , and 0V in VCCx.
Can someone suggest me some tricks ? I read on datasheet it is useful to put a diode between Vin and Vcc to prevent reverse discharge of VCCx when it is higher than Vin.
Thank
Regards
Simone